To make our site as user friendly as possible we use cookies. Please confirm that you agree to our use of cookies by clicking Yes.
FOR IMMEDIATE RELEASE No. 3215
Will enhance indoor lighting with sky-like depth and colors adjusted to time of day to make indoor spaces feel larger and more open
TOKYO, September 27, 2018 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has developed an indoor lighting technology that mimics the daily change of natural light from sunrise to blue sky to sunset. The system, which consists of a thin panel and frame measuring less than 100mm, incorporates a proprietary edge-lit method that emits LED light from the side of the light panel to achieve highly natural light with the depth and color of the sky. Mitsubishi Electric will exhibit its new technology during CEATEC JAPAN 2018 at the Makuhari Messe exhibition complex in Chiba, Japan from October 16 to 19. The timing of the envisioned commercial release will be announced later.
Prototype simulating blue sky
Basic structure of prototype
Sample application as skylights
Sample application as skylights and windows
Modern workplaces are being upgraded to create comfortable environments that stimulate and motivate employees. This includes the enhancement of lighting in offices that have darkened or covered windows or no windows altogether. Mitsubishi Electric's new system, unlike conventional LED lighting system, produces highly natural light, including colors similar to those of sunrises and sunsets as well as blue skies, and creates a sense of depth to make indoor spaces feel larger and more open.
Going forward, Mitsubishi Electric will develop applications that provide pleasing natural-like light in offices, public facilities and other environment where natural light is limited or unavailable.
Note that the releases are accurate at the time of publication but may be subject to change without notice.