To make our site as user friendly as possible we use cookies. Please confirm that you agree to our use of cookies by clicking Yes.
News Releases
FOR IMMEDIATE RELEASE No. 3309
TOKYO, October 3, 2019 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of a 12.1-inch WXGA TFT-LCD module designed for use in harsh outdoor environments, such as on construction sites and in heavy-duty vehicles, as well as in industrial applications and in agricultural use.
The new modules will offer an unprecedented combination of advanced features, including high-resolution WXGA (1,280 × 800 pixels), super-wide 176-degree horizontal/vertical viewing angles and a high luminosity of 1,500 cd/m2. They will additionally feature a high contrast ratio of 1,000:1, a versatile operating-temperature range of -40 to +80 degrees Celsius and will have high resistance to vibration, attributes for which there is increasing market demand.
Sample sales will commence October 31 through Mitsubishi Electric offices worldwide.
Mitsubishi Electric Color TFT-LCD Module
AA121TJ11
Product | Size | Resolution | Model | LED driver | Sample Shipments |
---|---|---|---|---|---|
TFT-LCD Module | 12.1-inch | WXGA | AA121TJ01 | Implemented | October 31, 2019 |
AA121TJ11 | Not implemented |
Note that the press releases are accurate at the time of publication but may be subject to change without notice.