To make our site as user friendly as possible we use cookies. Please confirm that you agree to our use of cookies by clicking Yes.
FOR IMMEDIATE RELEASE No. 3210
Market-leading touch functionality and sensitivity combined with max. 5mm cover glass
TOKYO, September 12, 2018 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of 7.0-inch WXGA and 15.0-inch XGA color TFT-LCD modules equipped with projected capacitive touch panels using cover glass of up to five millimeters in thickness. The new modules are designed for industrial application, including measurement system machine tools, construction, agricultural vehicles and factory automation, as well as gas station point-of-sale terminals. Sample sales will begin on October 31 via Mitsubishi Electric offices worldwide.
Mitsubishi Electric Color TFT-LCD modules with projected capacitive touch panel
The new modules will meet the increasing industrial demand for thicker and sturdier cover glass supporting operation by those wearing gloves. Accurate, multi-touch sensing is possible even when the screens are wet. Combining these cutting-edge touch panel capabilities with Mitsubishi Electric's proven TFT-LCD technology, the new models are built to handle a diverse range of applications and installation configurations.
Product | Model | Display Size | Resolution | Brightness (cd/m2) |
Shipment |
---|---|---|---|---|---|
TFT-LCD Modules with Projected Capacitive Touch Panels | AA070TA01ADA11 | 7.0-inch | WXGA | 800 | October 31, 2018 |
AA070TA11ADA11 | |||||
AA150XT02DDE11 | 15.0-inch | XGA | 600 | November 30, 2018 | |
AA150XT12DDE11 | 1200 | ||||
AA150XW01DDE11 | 400 | ||||
AA150XW14DDE11 | 800 |
Note that the releases are accurate at the time of publication but may be subject to change without notice.