To make our site as user friendly as possible we use cookies. Please confirm that you agree to our use of cookies by clicking Yes.
News Releases
FOR IMMEDIATE RELEASE No. 3361
TOKYO, June 16, 2020 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of its N-series 1200V SiC-MOSFET (silicon-carbide metal-oxide-semiconductor field-effect transistor) featuring low power loss and high tolerance1 to self-turn-on. The new series will help to reduce the power consumption and miniaturize power supply systems requiring high-voltage conversion, such as electric vehicle (EV) on-board chargers, photovoltaic power systems and more. Sample shipments will start this July.
Mitsubishi Electric will exhibit its new N-series 1200V SiC-MOSFET at major trade shows, including PCIM Asia 2020 in Shanghai, China from November 16 to 18.
N-series 1200V SiC-MOSFET
Product | Standards | Model | VDS | RDS(on)_typ. | IDmax@25°C | Package | Sample availability |
---|---|---|---|---|---|---|---|
SiC-MOSFET | AEC-Q101 | BM080N120SJ | 1200V | 80mΩ | 38A | TO-247-3 | July 2020 |
BM040N120SJ | 40mΩ | 68A | |||||
BM022N120SJ | 22mΩ | 102A | |||||
— | BM080N120S | 80mΩ | 38A | ||||
BM040N120S | 40mΩ | 68A | |||||
BM022N120S | 22mΩ | 102A |
Note that the press releases are accurate at the time of publication but may be subject to change without notice.