To make our site as user friendly as possible we use cookies. Please confirm that you agree to our use of cookies by clicking Yes.
News Releases
FOR IMMEDIATE RELEASE No. 3418
TOKYO, June 28, 2021 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it will soon begin operating the 5G OPEN INNOVATION Lab™ to collaborate with customers and partner companies on research and test demonstrations of "local 5G" private mobile communication systems. The 132-square-meter facility, based in the company's Information Technology R&D Center in Kamakura, Kanagawa Prefecture, will open on June 30. Mitsubishi Electric was recently licensed by the Ministry of Internal Affairs and Communications (MIC) to operate local 5G mobile communication systems designed for private use by municipalities and companies in designated areas to meet specific needs.
5G OPEN INNOVATION Lab
The lab's 4.8GHz-4.9GHz test environment will be used to research and demonstrate solutions for specific business, etc. needs from initial stages. In particular, they will perform comparative verifications of local 5G and other wireless methods, such as Wi-Fi 6 and private LTE, to determine the best communication method for each application and purpose.
The Ministry of Internal Affairs and Communications (MIC) sanctioned the private use of local 5G systems by enterprises and municipalities in December 2019, and then 4.6GHz-4.9GHz as a sub-6 GHz band for the construction of wide-area local 5G systems in December 2020. The environment in Japan is now ready for the deployment and expected growth of these private 5G systems and related solutions.
Mitsubishi Electric first launched a local 5G demonstration using millimeter-wave bands at its Nagoya Works in Nagoya, Aichi Prefecture in May 2020, and since then has been verifying the practical application of the technology for manufacturing.
Mitsubishi Electric will now open the 5G OPEN INNOVATION Lab to collaborate with customers and partners in using the 4.8GHz-4.9GHz sub-6 frequency range to address specific private communication needs, including through the development of related new 5G businesses and services. Customers and partners will be able to perform test demonstrations of potential business solutions using their own applications as well as those of Mitsubishi Electric, including for comparison with and evaluation against Wi-Fi 6, private LTE and other wireless systems.
Mitsubishi Electric aims to combine its own systems and equipment with local 5G systems in solutions that it will develop, build and provide on a one-stop basis. It also aims to create related new businesses and services in collaboration with customers and partners. In addition to studying various local 5G demonstrations, Mitsubishi Electric plans to conduct a wide range of test demonstrations at the lab, including the automatic and remote-control operation of mobile robots via 5G.
Note that the press releases are accurate at the time of publication but may be subject to change without notice.